Introduction
-------------
This text document accompanies the S-Video CCS test case for DM814X EVM. It 
provides a brief of the methodology of the test and the procedure for executing 
the same.

Overview
---------
This CCS test application validates the S-Video out present on the base board for its ability to send video data.
This test uses a tuner connected through a S-video cable.

Board settings
--------------
	This test case requires a tuner, S-video cable, VGA cable and a monitor.
	One end of the S-Video cable is connected to the S-video connector(JC1) of DM814X EVM and  the other end of the cable is connected to a tuner.
	Connect a VGA cable between the tuner and a VGA monitor.
	The monitor should be configured to S-Video mode (SV mode) with the help of tuner. 

Procudure
----------
This test application assumes the DDR controller initialization as well as all
the PLL initialization is already carried out by the GEL scripts. At the minimum
the following GEL scripts are to be executed.
	1. DM814X System Initialization --> BaseBoard_SVideo   

On executing the GEL script, a color bar pattern gets displayed in the VGA monitor. If the colour bar pattern gets displayed in the monitor, 
the test case is declared PASS otherwise the test is a FAILURE.